SAFEPARAM.ENCODERENDATTYPE
Description
Defines the type of safe encoder in the third encoder interface of theSMM.
This parameter can have the following values:
Value | Description |
---|---|
0 |
Unused |
1 |
EnDat 2.2 EQI 1131 |
2 |
EnDat 2.2 EQI 1131 |
To be used, the encoder interface must be linked to an axis (see AXIS#.SAFEPARAM.ENCODERSOURCE).
-
- EnDat encoders are not supported yet as safe encoders.
Context
Related safety parameters:
Versions
Action |
Version |
Notes |
---|---|---|
Implemented |
2-04-00-000 |
Implemented in SMM revision v0.56 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0, 1, 2 |
Default Value |
0 |
Data Type |
Integer |
Stored in Non-Volatile Memory |
No |